Graphics Editor Test Pane
Use the Test pane to test the dynamic behavior in Preview mode.
| Component | Description |
|---|---|
| Name | The name of the object you are testing. |
| Value | Tests a bind, that is, a dynamic behavior. Enter a value to start the test. |
| Unit Status | Tests the unit management under the condition that you have used getUnit in your scripts. Enter any text. |
| Status | Simulates signal status. "Value from device" is the normal status. |